As an alternative to the cable conduit, the project managers examined various solutions and finally came across the triflex® R energy chain. The 3D chain has been specially developed for robot applications. Together with the triflex® RS universal module, it was the perfect answer to the problems in the application. The particularly compact universal module is mounted on the robot at existing attachment points and can also be used in combination with the triflex® R chain in confined spaces. It ensures the energy supply to the robot head safely and without cable stress. Thanks to the retraction module, the universal module retracts the cable with every movement, so that the work area always remains free from now on. This has reduced downtime by two thirds (from an average of 55 to 7.5 faults per week). In addition, only 7-11 minutes of average maintenance work was required per week instead of 55 minutes. Even in the event of a major problem, maintenance is significantly simplified thanks to the modular design of the triflex®. The chain can be opened so that the cable and the feed cable no longer have to be laboriously removed at the ends when replacing them.
The results were so satisfactory that the use of the system for other BIW systems is also being investigated.