A yacht usually has another boat: a compact light boat or jet ski that takes passengers from the anchorage to land and back again. This is where a lift system, platform or garage comes into play.
H+B technics GmbH & Co KG is focussing on this market. Around 1,000 lift systems with load capacities of 350 to 2,500 kg are designed and built each year.
The first lift systems that H+B developed and built around twenty years ago are still in use today. This speaks in favour of the design as well as the individual components, including the energy supply. These have to be able to do a lot. For example, around two thirds of the lift systems are permanently under water, which is why they have to be extremely corrosion-resistant and therefore made of high-quality stainless steel.
Installation space is also an important issue, as space for the slewing drive is very limited.
Further requirements for the chain: they must be lubricant-free, maintenance-free and corrosion-free and generally achieve a long service life under adverse environmental conditions. A narrow bend radius is also important here.
And yet another H+B special solution is used for large yachts with garages. An overhead crane was developed and manufactured here, which picks up the boat and moves it into the parking position using a winch. To enable the crane's trolley to move, linear profile guides are required which, like the energy chain, should be seawater-resistant and maintenance-free. They should also require no lubrication and achieve a long service life under the special operating conditions. In addition, a low breakaway torque even after long periods of inactivity and a low weight are required.