Problem
The Schmid Group, headquartered in Freudenstadt, specialises in the development and manufacture of systems for photovoltaic and PCB production. The competence centre for handling technology is located at Schmid Technology Systems in Niedereschach. The product programme of this subsidiary includes loading and unloading systems. These systems separate PCBs, for example, which are arranged on cassettes, and feed them to a processing station via a conveyor belt.
The ever-increasing processing speeds and customer demands for greater flexibility have led to the development of a whole new generation of handling systems. While linear units were previously used to move the individual axes, a six-axis robot is now being used for the first time, which can load and unload cassettes with PCBs with cycle times of less than seven seconds. However, the flexibility of the system is more important than its speed. Because the robot can be freely programmed, a wide variety of movement patterns are possible - without any modifications or interventions in the hardware. For example, cassettes can be loaded and unloaded at different angles of inclination. The system is completely enclosed because PCB handling places the highest demands on cleanliness. Compactness therefore plays a major role - in cleanroom technology, cubic centimetres are the norm.
An interesting detail of the system is the gripper, which automatically recognises the size of the respective circuit board. The carrier plate with the vacuum grippers is made of weight-saving carbon fibres so that a compact 16 kg robot can be used and handling goods weighing up to 7 kg can be moved.