The decision was made in favour of an e-chain® of type E 4.12, which has also proven itself in other types of construction machinery. This type of chain is exceptionally robust. This is due in part to the rear grip, which ensures high lateral stability. This is particularly important when the mast tilts sideways because the drill head is positioned at an angle. The large diameter of the two hydraulic hoses for driving the drill gives an impression of the forces that the energy chain has to withstand in normal construction site operation. In addition, the hoses, which have a considerable dead weight, move when pressurised.
The signal cables, which are guided in a separate chamber, are less demanding in this respect. However, UV radiation, cold and temperature differences are factors that can have a negative impact on service life. This is why KGS Keller plays it safe here too and uses cables from the chainflex® range, which, like the energy chain, have been developed from the ground up for use in mobile applications and under unfavourable conditions.
The maximum mast height of the KB 6 - the name of the drilling rig, which is currently being manufactured in a small series - is 36 metres with an auxiliary mast. The chain travels on the mast over a distance of 8.10 metres, the trough finishes the basement itself. As the protective cage on the drill head is folded downwards in the travelling position, the chain must be flexible in both directions where the cage is folded through 90 degrees. This is not a problem with the E4 chain: so-called reverse bend radius elements are simply used in the respective zones. The abbreviation stands for 'reverse bend radius'. Three of these elements are installed in the chains of the new generation of Keller drilling rigs.