The Turomas-Tecnocat Group has dedicated itself to the construction of machines for the glass cutting process. While the company's glass cutting machines could previously only process glass with a maximum length of 6 metres, this system is the first in the world to store, transport and process workpieces as long as 12 metres.
The huge glass processing machine consists of an automated warehouse, an overhead loading station with suction cups, a swivelling table that picks up the glass from the loading station and sends it to the cutting table, as well as two swivelling and synchronised unloading tables for picking up the glass.
Both the cutting tables, or more precisely the bridge and the cutting tool, and the overhead loader required an energy chain for safe cable routing. Due to the long travel distances, particularly long chain versions were required that could also cope with the high acceleration and speed of the cutting table's linear motors. Due to the dimensions, these should be as lightweight as possible and still ensure stable but also low-noise movement.
As the loading station rotates around itself for transport from the bearing to the cutting table, it should be equipped with a rotating cable guide.
Overall, the aim was to create a system that guarantees high productivity and reliability at low cost.