Solution
The biggest problem with the concept for this storage and retrieval unit was the fast movements that take place in 3-dimensional space. To prevent the abrupt horizontal, vertical and diagonal movements from creating a tangle of cables, all data and supply lines are routed in an igus ® e-chain®, which rolls up and down on an e-spool®. As an alternative to the cable drum, the e-spool® can be used gently and safely with energy chains and cables. It is used in particular when many different cables need to be routed in a confined space. A standard e-chain® is guided by a roller and, thanks to an integrated retaining spring, ensures that the energy supply system is always exactly the right length and tension. In the starting position, the e-chain® space-saving is completely rolled up. The twister band connects the reel to the shaft end block, which serves as an interface to the permanently installed cable.