The robot was created in a joint development project with Fanuc and makes it possible to combine materials such as aluminium, aluminium alloys, copper, titanium and steel, which are normally difficult to weld together. What's more, no additional material is required. The materials are joined together by pressure and friction alone. This closed connection is so superior to the base materials that bending the weld seam by even 90° is no problem.
Company: FPT INDUSTRIE SPAContact person: Sig. Sebastiano CarlessoCountry: Italy