Change Language :
The GS-series of machining centres from Alzmetall is characterised by high dynamics and precision; it is mainly used for demanding machining tasks in high-volume production, tool and mould making, prototype construction and in the aerospace industry. Alzmetall has found an economical and technically convincing solution for the energy supply to the spindle: A customised, ready-to-install energy chain system is purchased from igus®.
Also ideal for maintenance and retrofitting
Two variants were specified for the chain configuration: one for the standard versions of the GS 650, a second with additional cooling hoses for the more powerful spindle with 30,000 rpm. igus® delivers these variants, which are assembled in Cologne, to Altenmarkt "just in time". Of course, further cables can be integrated into the chain if required. This can even be done retrospectively: Another argument that convinced the Alzmetall designers is the simple retrofitting of the energy chain, for example if additional axes or minimum quantity lubrication is required. In this case, you simply snap on the individual chain links and insert the cable into the channel provided.
The readychain®-energy chain in Alzmetall's production halls is hard to miss: The fully assembled chain and power packs, including the distribution box, take up barely more storage space than a Euro pallet. To keep an eye out for other igus® products used by Alzmetall, you have to walk very carefully through the assembly area in Altenmarkt - and you will find them: iglidur ® plain bearings made of high-performance polymers with "built-in" lubrication are used in the holders of the tool magazines.
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr