Cinetic Landis Ltd. finally decided in favour of e-chain®, more specifically the E6 energy chain series from igus®. However, before the machine manufacturer found the final solution for its system, it looked at the e-chain® 1640, which was found to be too heavy, stiff and prismatic in its design for the company's specific application. In the end, igus® offered the mechanical engineer a sample of the E6 chain as a counter-design for internal visualisation of the dimensions and precise functionality.
From this point, it was not far from the model to the actual implementation in the system, as the E6 was able to completely convince Cinetic Landis. The chain offers the user a number of advantages: In addition to the chain's high degree of flexibility, dispensing with a traditional prismatic design has enabled smoother movement, which also ensures more precise operation of the grinding machine. In addition, the E6 chain is not affected by the lubricating oil used during sanding. This means that there is no bolt/bore connection for connecting the chain components and wear and tear cannot occur here. Furthermore, only minimal support was required for the energy chain, which consists of just two steel rods. Even an unsupported chain section of approx. 1 metre in between, which reduces the friction of the entire installation, can be supported by the chains without any problems. Finally, the 230° rotating movement of the chain is a "simple" rotating movement, and not a movement with a reverse bend radius. This keeps the costs low, the application as clear and the maintenance as simple as possible.