Blatchford is an English manufacturer of prostheses that uses the latest technologies in the industry to help people around the world with mobility impairments in everyday life. The focus is on the development of foot and leg prostheses that are designed to help users regain this mobility in the best possible way.
This also applies to the "TT Pro", an adapter for leg prostheses that can be used not only in everyday life, but also for sporting activities such as golf. This is because the prosthetic element can allow torsion thanks to an integrated spring, thereby protecting the socket from the shear forces that occur in a sporting environment. This not only enables complex movements, but also protects the user's joints and spine.
The bearings installed in the prosthesis must also be able to permanently follow these movement patterns, absorb the high forces, exhibit low wear and, despite their stability, also offer flexibility in order to provide the user with the best possible comfort experience.