The challenge was cleverly solved with an igus® e-chain® from the E2/000 series: If you turn it by 90° and stand it on end, it can follow the longitudinal movement of the stacker crane over a length of 12 metres and perform a curved movement at the same time. Equipped with lateral sliding elements that protect against wear, the E2 travels on a stainless steel guide that specifies the desired radius when cornering. With the unusual upright position of the e-chain®, it was important to equip it with locking dividers instead of the usual sliding crossbar. This is because they prevent the crossbar and cable from moving downwards due to gravity and lying on top of each other. As the E2 can be easily clipped on and individual cables can be quickly replaced or added, the system also scores highly in terms of ease of maintenance.