The main challenge in this project for our customer was that the cable route through the machine from the consumer to the control cabinet was 100 metres. This poses logistical challenges in the event of servicing, where there are planned or unplanned downtimes. On the one hand, a pre-assembled energy chain with 100 metres of cable including intermediate connection points could be ordered and this correspondingly heavy system could then be routed through the hall, which takes a lot of time and effort during installation. Alternatively, individual parts can be purchased, which are lighter and easier to handle, but in turn lead to additional work and are prone to errors during installation and completion. There is also a loss of production during the installation time.
In addition, the customer's four machines work independently of each other. However, they are connected to each other via a safety circuit. If one machine breaks down, all four machines are stopped. This is why it is so important for our customer to be able to safely replace the entire energy chain in the event of a machine standstill, thus saving valuable time.