Avoid reduced press fit due to anti-corrosion agent
iglidur® bearings were tested in combination with various corrosion protection agents
Initial situation
If a bearing position is to operate 100 % lubrication-free, it may be advisable to treat the bearing seat with an anti-corrosion agent. These agents may reduce the seizure of the bearing.
Test: displacement force with different anti-corrosion agents
The test shows that almost all anti-corrosion agents reduce displacement force. Only TectylTM 300G Clear E enhances press fit.
Result: TectylTM 300G Clear E under the influence of motion and force
Even under the influence of force and movement, TectylTM 300G Clear E can achieve a higher tight fit of the bearing. In the test, it is almost twice as high as with the plain bearing without anti-corrosion agent.
Largest test laboratory in the industry
We carry out tests so that you don't have to. Find out how our iglidur plastic bearings are tested in the largest test laboratory in the industry. We also carry out individual customer tests here.
Here, you can find answers to the most important questions regarding iglidur plain bearings. Compiled and answered in detail by our experts for plain bearing technology.