The system with the designation "Autocap RT" is used in Dromont dispensing machines and has the function of automatically closing the dispensing head of the machines after each dispensing process. This protects the nozzles and the liquid remaining in them from drying out at the end of dispensing. The system then opens the head again automatically with the next dispensing command. Closure is achieved by the movement of a special cap equipped with a humidification system. This is placed under the nozzle area of the dispensing head to create a closed and humid environment. The contents are kept liquid while a seal is pressed around the edge of the head. This creates a suitable seal that prevents the dispersion of the moist atmosphere thus created.
The Dromont vending machines in which the system is used are used in a variety of areas:
- in shops and shopping centres open to the public (e.g. paint shops, Brico and various DIY stores)
- in industrial environments as stand-alone dosing devices
- in industrial environments as components of dosing systems
In all cases, the operating conditions are generally in an ambient temperature range of 15°C to 30°C and in a potentially dirty atmosphere that can easily contain fine dust, at least inside the machine.
Furthermore, the following challenges had to be overcome:
- vertical displacement and horizontal movement with a single drive
- Enabling the most effective and uniform sealing possible with the head closed
- Fast actuation (less than 1 second)
- very low actuating force
- easy adjustment during installation
- complete absence of maintenance work
- reliability over the entire service life of the machine (more than 10 years)
- small overall dimensions
- noiselessness
- low costs