Change Language :
Eleven floors and the basement area are served by a group of lifts in a Sparkasse building. Not all floors are accessible to customers. They are controlled by an access control system. The required bus signals are transmitted via a special cable which, due to its design, can demonstrably withstand the high tensile strain caused by the freely suspended application in the long term.
"Our contact person suggested that we use an extremely robust bus cable for long, suspended travels from the industrial environment," recalls Krauß. "At the time, however, it was still in the test phase. Nevertheless, we decided to use it. And we haven't regretted that decision once."
"We manufacture cables for almost every application, using a wide variety of materials and processes," explains igus® Product Manager Andreas Muckes. "Depending on the design, this is possible from lengths of 500m." A wide variety of cables are tested in the company's own laboratory, particularly with regard to their dynamics over long and short distances. Radii and torsion also play an important role. The focus is always on the right cable concept for demanding movements. Over 2 billion test cycles are realised every year for research and development.
Due to their weight and the lack of a supporting element, normal bus cables cannot be used as they only withstand loads of up to 15N/mm². All in all, the facts show that the cable length could be more than 1km free-hanging without any loss of performance. "For us, this means that we could theoretically extend the building significantly," says the Head of Building Organisation at Sparkasse. An additional cable was initially installed in the lift system to be on the safe side and to be able to carry out measurements of the occurring data set. The frequency of the lifts is very high. Just under six months after the system was commissioned, 56,970 trips had already been recorded. Two years later, they exceeded the 160,000 mark without any faults being recorded. "The approval limit will certainly not be reached; it's more likely for a new lift control system to be installed," so igus® Sales Consultant Eugen Kowalczyk. chainflex® cables for industrial applications are designed for very small bend radii, high numbers of cycles, speeds, accelerations and demanding environmental conditions.
This cable is a customised solution that has been developed to meet the highest requirements. However, all our experience is incorporated into the wide range of chainflex® standard products. This means that the customer is always on the safe side and gets the right cable for every requirement profile.
You can find more interesting applications from a wide range of areas here
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr