Non-destructive material testing: In order to couple ultrasonic waves into the material, a coupling agent is used in conventional ultrasonic testing methods. A special device technology makes it possible to dispense with this coupling agent, which means that testing with so-called airborne ultrasound is not only contactless, but new materials such as lightweight construction materials can also be tested.
One of the aims of the "IfUS" research project (funded by the BMBF) was to develop a transportable and flexible scanning machine for testing plate and complex freeforms with airborne ultrasound. The result was the "PortUScan 460". The scanner was to be as flexible, small, light and therefore mobile as possible while maximising the scanning area so that large or heavy objects could be inspected outside the laboratory with little effort. A certain robustness of the parts was required for possible industrial and outdoor applications.
Alternative bearing designs based on roller bearings, ball screws or metal worm gears were usually too massive and therefore too large and heavy, as they were intended for milling technology, for example. The weight of the scanner would have been excessively increased and the possible applications limited.