Inside the Camping Butler is a tray into which the cassette is inserted manually. Once the cassette has been inserted, the side walls of the tray adjust to the waste-holding tank with the help of two precision shafts mounted on bearings, so that the cassette is fixed in the tray. Furthermore, e-chain® ensures a safe energy supply. A drylin® room linear robot with two Z-axes is mounted on the tank itself. This complete system is supplied and assembled with motors, coupling and encoders. It consists of two drylin® ZLW toothed belt axes, one ZLW cantilever axis and two ZLW Z-axes. The slides of the linear guide are equipped with lubrication-free sliding elements that ensure precise guidance.
Fully automatic and simple operation Once the faeces tank has been inserted, the lid of the cassette is unscrewed and opened using a gripper mounted on one of the Z-axes of the gantry. Connected to the second Z-axis, an attachment is placed on the opening of the cassette through which water is filled. A gear rotates the tray and the gantry through 180 degrees to empty and rinse the contents of the cassette. The gear returns the tub to its original position, the flap opens and the camper can remove the cleaned cassette.