igus products and PFAS

igus products are PFAS-free

The most important facts in brief

  • Many of our materials do not contain PTFE.
  • According to the OECD, materials with PTFE are "products of low concern" (non-toxic and non-bioaccumulative). No traces of more than 100 of the most critical PFAS compounds could be detected in these materials.
  • If PTFE is not banned, our materials are generally not affected.

Background: What are PFAS?

Classification of PFAS
Classification of PFAS

Non-polymers

Polymers

  • Fluoropolymers consist of a carbon chain with directly attached fluorine atoms. This makes them so stable that they cannot decompose into toxic substances. According to the OECD, fluoropolymers are "products of low concern", non-toxic and non-bioaccumulative, i.e. they cannot accumulate in organisms. The only risk is the possible use of toxic additives during production in the form of emulsifiers. Fluoropolymers are used, for example, in coatings, seals and cable insulation. Fluoropolymers include PTFE, among others.
  • Polymers with fluorinated side chains also consist of a carbon chain, but with side carbon chains to which the fluorine atoms are attached first. As a result, these polymers are less stable and there is a risk of losing the side chains. They are used, for example, as impregnating agents.


What does a possible PFAS ban mean for igus products?

  • iglidur A160, A200, A230, A500, B160, B180, C, F, GLW, i230, J3, M250, R, T220, W160, X6
  • igumid G, GLW, NB, TE
  • iglidur A160, A181, A230, A350, A500, AX500, E7, F, F2, F300, G, G1, GLW, H1, H2, H370, H4, i3, i6, J, J200, J3, J350, K230, L100, L250, M250, P, P210, Q2, Q290, W300, X, Z
  • igumid CG, ESD, G, GLW, NB
  • igutex TX1, TX2, TX3
  • RN312

Further information on our products and PFAS

White paper: focussing on PFAS

PFAS in focus: planned restrictions, challenges and solutions for the industry