The UB-Space team developed a special mechanism for the rocket module in order to be able to reliably eject this FFU at the right time. However, the use of the mechanism in space differs significantly from normal missions on Earth. According to ship technology student Oliver Dorn, energy consumption, weight and installation space are all limited. In addition, the air friction results in temperatures of up to +200 °C. After several tests, the team decided in favour of a drive system consisting of two parallel threaded spindles that extend the unit in which the FFU is located. A flap, which is blasted off beforehand, serves as the opening for the unit. The stainless steel spindles from the igus® drylin® programme are each driven by a NEMA 11 stepper motor. They cover a distance of 150 millimetres at a high torque and low speed of 3 cm/s. The opposite side of the construction is mounted on the rocket wall with a 3D-printed lead screw nut made of iglidur® J260-PF. So that the FFU can be ejected as smoothly as possible, the ejection chute is lined with the Tribo-Tape plastic sliding film made of iglidur® V400. The materials from igus® are ideally suited for precisely this type of application, as their optimum sliding properties ensure tilt-free and energy-efficient ejection. They are also resistant to pressure and temperature and have a low weight, which was decisive for the special structural requirements.