Huisman, based in the Netherlands, specialises in the construction and maintenance of heavy construction machinery worldwide, e.g. for the renewable energy and oil production sectors.
One such "machine" from Huisman, the so-called Multi Purpose Tower, is used on drilling ships to perform the same functions as a conventional drilling rig. The huge scaffolding, which is used to guide the drill pipe and house other machinery, protrudes conspicuously from the ship due to its height. Due to its exposed position, the cable faced several challenges, e.g. for the energy supply and cable routing. Not only does this result in an enormous travelling length, which is associated with a high cable weight. The use on the high seas in rough winds also means that all cables must be routed safely and well protected.