Today, sheerleg cranes are irreplaceable for shipbuilding, but also for the realisation of other structures such as bridges. Equipped with an A-frame, offshore cranes can sometimes lift heavy loads of several thousand tonnes.
Absolutely reliable components must therefore be used to feed sensitive cables for power or data to the adjustable crane jib. In addition to typical offshore conditions such as aggressive corrosion and strong winds, there are other requirements depending on the design of the sheerleg crane. Particularly in the case of the large heavy-duty cranes, the travel distances are long and the cable weights to be moved are correspondingly high. For these two sheerleg projects, the planners were looking for a low-wear and permanently safe cable routing that could guarantee a high level of planning reliability.