My contact person
igus® GmbH

Spicher Str. 1a

51147 Köln

+49 2203 9649 0
INT(ES)

igubal® bearing elements application examples

igubal® bearing elements can be used without problems even in harsh environments and are maintenance-free. They are corrosion-resistant in humid environments. The operating temperature is from -30°C to +80°C. Seals are not necessary, even in extremely contaminated conditions. This is true for fine dust as well as coarse dirt.
Every year, igus® engineers develop more than 100 new plastic compounds and conduct more than 3500 tests on maintenance-free plain bearings every year, and thus over the years has established a large database of polymers' tribological properties.

Search from over 140 applications of our customers


In a wide range of industries, solutions are technically improved and costs saved by the use of igubal® bearing elements.


More applications

Test stand for control centres

Only extensive earthbound testing can demonstrate the suitability of components for space applications.

Plastic spherical bearings for electric wheelchairs

Lubrication- and maintenance-free plastic bearings provide the required functional reliability in electric wheelchairs.

Lubrication-free linear and spherical bearings for baked goods gripper

This gripper picks up freshly baked goods from a conveyer belt and packs them in baskets.

Plain and spherical plain bearings withstand strong vibrations in grain sorters

This machine cleans and sorts all types of grain. First the grain is separated from other material by an air current.

Bearing technology and energy chains for electric aircraft

To achieve the best flying conditions, all components must be lightweight and at the same time as durable as possible.

Bearing technology for Mars robots

This robotic vehicle is designed for a very special environment: it will one day be driving on Mars.

Plain and spherical bearings in the prosthetic joint

This joint is a new development to be used in prostheses. iglidur® J plain bearings and igubal® spherical bearings are installed in it.

Spherical bearing for solar aeroplane

The prototype of the „Sunseeker Duo“ solar plane is the world‘s first solar-powered two-seater.

Gritting unit

The screwconveyer of the gritting unit has to be mounted movable in order to compensate axial offset and dynamic movements in the screw.

Producción de CD y DVD

Las cabezas articuladas de plástico garantizan un funcionamiento intensivo del equipo.

Equipment manufacture

Lubrication-free tribopolymers in extreme application - Packaging unit for profiles.

Distribuidor de estiércol

Un test dinámico refleja una vida útil superior a 10 años.

Fully automatic tire fitting lines

No more expensive repairs

Bearing technology for helicopter drone

Light and free from play

Plain bearing for filling valve in beverage bottling plant

El desafío: la temperatura máxima de funcionamiento es de 140°C y los materiales utilizados deben resistir a todos los detergentes utilizados en el sector de las bebidas.

Bearing technology for ultra-light gyrocopters

El iglidur® G es la solución ideal para esta cabeza del rotor. Las hélices sustentadoras giran aproximadamente 400 veces por minuto y efectúan movimientos oscilantes de 30° máx.

Special bikes and therapeutic accessories

Plain, spherical and linear bearings made of plastic help to improve mobility and the quality of life

Soccer table

Application of a high-value spindle lift table with steep-threaded spindle, linear guide systems and igubal® spherical bearings.

PLC laboratory trainer

The aim of the concept is to demonstrate to the students how to handle a programmable logic controller (abbreviation: PLC) in an attractive way.

Máquina para formar, llenar y sellar bolsas continuas

A pesar de todas las influencias exteriores, los Cojinetes de deslizamiento de plástico libres de mantenimiento aseguran el periodo de funcionamiento necesario.

Bearing technology, energy chains and cables for straightening machine

Quick, straight, precise: this is how the requirements in sheet metal machining can be summarized. Sophisticated straightening technology makes all this possible.

Bag forming, filling and sealing machine: Hygienic design of the format adjustment

On these horizontal forming, filling and sealing machines, the total freedom from maintenance over the machines' entire life cycle was particularly important for the customer.

Cow cleaner

Lubrication-free polymer bearing technology for cow cleaners


Los términos "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" y "yes" son marcas comerciales legalmente protegidas de igus® GmbH en la República Federal de Alemania y otros países. Esta es una lista no exhaustiva de las marcas comerciales de igus GmbH o de empresas afiliadas de igus en Alemania, la Unión Europea, EE.UU. y/u otros países o jurisdicciones.

igus® GmbH puntualiza que no vende ningún producto de las empresas Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber y cualquier otro fabricante mencionado en esta página web. Los productos que ofrece igus® S.L.U. son los de igus® GmbH.